Part Number: TMS570LS1227
Hello,
a colleague of mine is working with the TMS570LS1227. In his test environment the TMS570 is acting as an SPI slave and it is connected (via SPI) to an IMX6 CPU Board, acting as an SPI Master. TMS570 and IMX6 are embedded in the same CPU board and have the power supply in common.
After flashing the SW on the microcontroller, the SPI communication works fine unless he needs to reset the board. After a reset, he reports
<< If I turn off the motherboard, and after a subsequent power on, the communication via SPI fails and is not restored.
It is necessary to load the microcontroller software again to restore communication.>>
Do you have any idea about the problem?
Thanks