Part Number: TMS570LC4357
Other Parts Discussed in Thread: TPS62160-Q1
Good Morning,
I am designing a new board with TMS570LC4357-Q1 and I am guessing about the current consumption. In the datasheet I see a 510mA typ and a maximum of 990mA.
Where is all this difference coming from? Is it a transient or it refers to full operating capabilities? Or is it the worst case in temperature and voltage supply?
The typical 510mA is in full operating at standard temperature or in a different operating condition?
All theese questions because I would like to supply the MCU with two 1-A Buck controller TPS62160-Q1 (1V2 and 3V3) and I am not sure if it is enough.
Hope you can clarify my doubt.
Thanks in advance,
Dario Moscardi