Other Parts Discussed in Thread: TLIN1027-Q1
Hi,
We are in the process of designing OBD. Do you have any controller which supports all the protocols stated below:
SAEJ1850
ISO14230
ISO 9141 - 2
ISO 15765 CAN
Please share your thoughts on following queries:
1.Do you need a dedicated module on controller other than transceiver to Interface J1850 (VPW AND PWM)?
2.Can we use normal SCI/UART for K line and L Line protocol.
3.Is there any thing such as K Line UART like (CAN TX and RX - CAN DEDICATED UART), is dedicated UART available for this protocol.
4.Please suggest suitable transceivers if you have.
5.Please share reference designs and App notes with the Infor regarding the designing of OBD Protocols.