This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS3137: ADC/N2HET interface

Part Number: TMS570LS3137

Tool/software: Code Composer Studio

I am wondering if the ADC and N2HET interface can be used in the TMS570LS3137 de development kit. Or is there any development kit of TMS570LS serial equipped with ADC and N2HET interface on the board. I am selecting some to buy. Thank you!

  • Hi Jiayi,

    Yes, the ADC signals and N2HET signals are routed to the connectors. You can use those signals on the connectors without any issues. There is a capacitor footprint between each ADC pin and GND, so you can populate a capacitor to the ADC pin if needed.

    We don't have daughter card for the development kit (HDK).