Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

EK-TM4C129EXL: FreeRTOSConfic file for Launchpad board?

Part Number: EK-TM4C129EXL

Hello all,

I know TI does not support FreeRTOS anymore (I'm not happy about that BTW), but does anyone have a working FreeRTOSConfig.h file that I can use for the EK-TM4C129EXL board?  The only closest one FreeRTOS has is for the MSP432, and I know nothing about that one.  BTW, this needs to be for FreeRTOS rev V10.3.1

Thanks George

  • Hi George,

      Here is the FreeRTOSConfig.h for v7.0.2 that I found for the Tiva device. For the complete FreeRTOSConfig.h customization options, please go to this link. https://www.freertos.org/a00110.html

    /*
        FreeRTOS V7.0.2 - Copyright (C) 2011 Real Time Engineers Ltd.
    
    
        ***************************************************************************
         *                                                                       *
         *    FreeRTOS tutorial books are available in pdf and paperback.        *
         *    Complete, revised, and edited pdf reference manuals are also       *
         *    available.                                                         *
         *                                                                       *
         *    Purchasing FreeRTOS documentation will not only help you, by       *
         *    ensuring you get running as quickly as possible and with an        *
         *    in-depth knowledge of how to use FreeRTOS, it will also help       *
         *    the FreeRTOS project to continue with its mission of providing     *
         *    professional grade, cross platform, de facto standard solutions    *
         *    for microcontrollers - completely free of charge!                  *
         *                                                                       *
         *    >>> See www.FreeRTOS.org/Documentation for details. <<<     *
         *                                                                       *
         *    Thank you for using FreeRTOS, and thank you for your support!      *
         *                                                                       *
        ***************************************************************************
    
    
        This file is part of the FreeRTOS distribution.
    
        FreeRTOS is free software; you can redistribute it and/or modify it under
        the terms of the GNU General Public License (version 2) as published by the
        Free Software Foundation AND MODIFIED BY the FreeRTOS exception.
        >>>NOTE<<< The modification to the GPL is included to allow you to
        distribute a combined work that includes FreeRTOS without being obliged to
        provide the source code for proprietary components outside of the FreeRTOS
        kernel.  FreeRTOS is distributed in the hope that it will be useful, but
        WITHOUT ANY WARRANTY; without even the implied warranty of MERCHANTABILITY
        or FITNESS FOR A PARTICULAR PURPOSE.  See the GNU General Public License for
        more details. You should have received a copy of the GNU General Public
        License and the FreeRTOS license exception along with FreeRTOS; if not it
        can be viewed here: www.freertos.org/a00114.html and also obtained
        by writing to Richard Barry, contact details for whom are available on the
        FreeRTOS WEB site.
    
        1 tab == 4 spaces!
    
        http://www.FreeRTOS.org - Documentation, latest information, license and
        contact details.
    
        http://www.SafeRTOS.com - A version that is certified for use in safety
        critical systems.
    
        http://www.OpenRTOS.com - Commercial support, development, porting,
        licensing and training services.
    */
    
    #ifndef FREERTOS_CONFIG_H
    #define FREERTOS_CONFIG_H
    
    /*-----------------------------------------------------------
     * Application specific definitions.
     *
     * These definitions should be adjusted for your particular hardware and
     * application requirements.
     *
     * THESE PARAMETERS ARE DESCRIBED WITHIN THE 'CONFIGURATION' SECTION OF THE
     * FreeRTOS API DOCUMENTATION AVAILABLE ON THE FreeRTOS.org WEB SITE.
     *
     * See www.freertos.org/a00110.html.
     *----------------------------------------------------------*/
    
    #define configUSE_PREEMPTION                1
    #define configUSE_IDLE_HOOK                 0
    #define configUSE_TICK_HOOK                 0
    #define configCPU_CLOCK_HZ                  ( ( unsigned long ) 50000000 )
    #define configTICK_RATE_HZ                  ( ( portTickType ) 1000 )
    #define configMINIMAL_STACK_SIZE            ( ( unsigned short ) 200 )
    #define configTOTAL_HEAP_SIZE               ( ( size_t ) ( 30000 ) )
    #define configMAX_TASK_NAME_LEN             ( 12 )
    #define configUSE_TRACE_FACILITY            1
    #define configUSE_16_BIT_TICKS              0
    #define configIDLE_SHOULD_YIELD             0
    #define configUSE_CO_ROUTINES               0
    #define configUSE_MUTEXES                   1
    #define configUSE_RECURSIVE_MUTEXES         1
    #define configCHECK_FOR_STACK_OVERFLOW      2
    
    #define configMAX_PRIORITIES                16
    #define configMAX_CO_ROUTINE_PRIORITIES     ( 2 )
    #define configQUEUE_REGISTRY_SIZE           10
    
    /* Set the following definitions to 1 to include the API function, or zero
    to exclude the API function. */
    
    #define INCLUDE_vTaskPrioritySet            1
    #define INCLUDE_uxTaskPriorityGet           1
    #define INCLUDE_vTaskDelete                 1
    #define INCLUDE_vTaskCleanUpResources       0
    #define INCLUDE_vTaskSuspend                1
    #define INCLUDE_vTaskDelayUntil             1
    #define INCLUDE_vTaskDelay                  1
    #define INCLUDE_uxTaskGetStackHighWaterMark 1
    
    /* Be ENORMOUSLY careful if you want to modify these two values and make sure
     * you read www.freertos.org/a00110.html first!
     */
    #define configKERNEL_INTERRUPT_PRIORITY         ( 7 << 5 )    /* Priority 7, or 0xE0 as only the top three bits are implemented.  This is the lowest priority. */
    #define configMAX_SYSCALL_INTERRUPT_PRIORITY     ( 5 << 5 )  /* Priority 5, or 0xA0 as only the top three bits are implemented. */
    
    #endif /* FREERTOS_CONFIG_H */