Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS570LS3137: MibSPI and EMIF Module Test

Part Number: TMS570LS3137

Tool/software: Code Composer Studio

How to test mibspi and emif?Do I need to connect external devices?

  • Hello,

    TMS570LSx MibSPI modules support internal loopback and I/O loopback test modes. The internal loop-back self-test mode can be utilized to test the SPI transmit and receive paths. Input/Output Loopback Test mode supports the testing of all Input/Output pins without the aid of an external interface.

    To test EMIF, you need to connect an external memory device to EMIF interface.