Part Number: EK-TM4C1294XL
Tool/software: Code Composer Studio
This may be a simple code question, or something else. C is still somewhat uncharted territory for me.
I a trying to read in a 32 bit binary word from GPIO ports. (seems to work)
And then send that word onto ethernet using UDP..
However, there seems to be a problem preparing the data for UDP.
I have this code below:
int main(void)
{
int Indicator;
struct pbuf* pdat = pbuf_alloc(PBUF_TRANSPORT,40,PBUF_RAM);
u32_t data;
Setup();
Indicator=0;
while (1) {
data=Get32();
memcpy(pdat->payload,&data,4);
Indicator^=4;
GPIOPinWrite(GPIO_PORTN_BASE,GPIO_PIN_2,Indicator);
}
}
The code compiles but crashes at run time immediately after the memcpy instruction. Comment that line out, and the rest runs OK.
I suspect something not quite right around my use of the pointers involved, but ...
Below is, what the disassembler tells me:
main():
00000f44: 2000 movs r0, #0
00000f46: B538 push {r3, r4, r5, r14}
00000f48: 2128 movs r1, #0x28
00000f4a: 4602 mov r2, r0
00000f4c: F7FFFB82 bl pbuf_alloc
00000f50: 4605 mov r5, r0
333 Setup();
00000f52: F7FFF955 bl Setup
335 Indicator=0;
00000f56: 2400 movs r4, #0
338 data=Get32();
$C$L4:
00000f58: F7FFFFD6 bl Get32
339 memcpy(pdat->payload,&data,4);
00000f5c: 466A mov r2, r13
00000f5e: 6869 ldr r1, [r5, #4]
338 data=Get32();
00000f60: 9000 str r0, [r13]
339 memcpy(pdat->payload,&data,4);
00000f62: 6812 ldr r2, [r2]
00000f64: 4608 mov r0, r1
00000f66: 6002 str r2, [r0]
343 GPIOPinWrite(GPIO_PORTN_BASE,GPIO_PIN_2,Indicator);
00000f68: 4803 ldr r0, [pc, #0xc]
00000f6a: F0840404 eor r4, r4, #4
00000f6e: 2104 movs r1, #4
00000f70: B2E2 uxtb r2, r4
00000f72: F000F93F bl GPIOPinWrite
337 while (1) {
00000f76: E7EF b $C$L4
The crash happens at address 0x0F68, at which time, the processor jumps to some default FaultISR for an eternal loop.
I know too little (near to nothing, actually) about the assembly code for this processor to fully understand, what is going on. x86 code would have been another matter.
LATEST update:
The instruction at 0x0F66 apparently tries to drop something at the address set aside for ResetISR !!!
That does NOT seem right. There is not any RAM there, I think.