Tool/software: Code Composer Studio
Hello!
I work on project where custom board based on TM4C129K MCU is connecting to external device via TCP/IP. The traffic is rather big - device sends me data at up to 125kb/sec, but controlling traffic from my board to device is not big.
Rarely (about once per couple of days) I got hard fault inside tcp_output() function:
if (TCP_TCPLEN(seg) > 0) {
seg->next = NULL;
/* unacked list is empty? */
if (pcb->unacked == NULL) {
pcb->unacked = seg;
useg = seg;
/* unacked list is not empty? */
} else {
/* In the case of fast retransmit, the packet should not go to the tail
* of the unacked queue, but rather somewhere before it. We need to check for
* this case. -STJ Jul 27, 2004 */
if (TCP_SEQ_LT(ntohl(seg->tcphdr->seqno), ntohl(useg->tcphdr->seqno))) {
/* add segment to before tail of unacked list, keeping the list sorted */
struct tcp_seg **cur_seg = &(pcb->unacked);
while (*cur_seg &&
TCP_SEQ_LT(ntohl((*cur_seg)->tcphdr->seqno), ntohl(seg->tcphdr->seqno))) {
cur_seg = &((*cur_seg)->next );
}
seg->next = (*cur_seg);
(*cur_seg) = seg;
} else {
/* add segment to tail of unacked list */
useg->next = seg;
useg = useg->next; // <---- HERE!
}
}
/* do not queue empty segments on the unacked list */
} else {
tcp_seg_free(seg);
}
seg = pcb->unsent;
in the line
useg = useg->next;
and useg here is ether 0 of corrupt.
Asked on lwip support forum, but they said the version of lwip is old and is a port by TI, so I should ask TI engineers.
Currently device is stopped in debug state right after hard fault, so I can browse any variables or memory.
The heap state at time of fault is ok, as I embedded heap checking in hard fault ISR.