Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: TMS570LS317 parity error In DCAN

Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN

TMS570LS317 parity error:

Hello Support team,

I have a problem with DCAN in TMS570LS317 with the parity check. At the beginning I make a hardware init with MSINENA and minitgcr and the message Ram is initialized (0xFF1E0000 and the others). After that I go to make the init of the DCAN: the mailboxes and everything in the CAN controller, in the init I activate the parity check PMD (!= 5), when I try to initialize the IF1 and IF2 (I tried to write any value), a parity error occurs,  after a reset Can controller, the parity error goes away, but when I try later to start sending (I write in IF_CMD after after filling the data), I get a parity error and interrupt. The parity error is in the register 0xFFF7DC04.

Could you please tell me if my steps are wrong, what causes the issue and what is the best way to make the whole initialization without any parity issue.

I'm using WinIDEA 2012 and iSystem debugger.

Thank you very much for your help.

Best Regards.

Rostom

  • Hi Rostom,

    The parity check should be enabled before initializing the CAN message objects.If the parity check is disabled, the parity bits in message RAM will be left unchanged on write access to data area. After the parity check is enabled, you will get parity error when reading the data from message RAM.

  • Hi,

    Thank you very much for your response but that's exacly what I do and what I know, if it's possible I need more details.

    I will describe for you the exact situation:

    At first in the starup code I initilize the PLL WD and eveything related to HW and I initialize the Message RAM with MSINENA and MINITGCR, then I wait for the status bit so all message Ram are initilized.

    After that I go to initilize the CAN controllers(DCAN1, DCAN2 and DCAN3), I activte the PMD register for enabling the parity check, I start initializing the message ram again with my needed values using IF, when I write to CMD register in the interface IF, a parity error occures directly. 

    I go to initilize the other channels and the same behaviour occures, after each software reset, the parity error disappears.

    After the init I want to write a message using IF, when I write CMD register to start the transfer from IF to message RAM, a parity error occurs again and I get an interrupt.

    What could be wrong in this situation and what is the best way to initilize everything and writing in IF without getting a parity issue?

    Thank you very much for your response.

    Best Regards,

    Rostom

  • Hi Rostom,

    Did you perform CAN parity check to test the parity mechanism?  --->     can1ParityCheck();

    Your configuration looks fine. This is my test: the parity is enabled before any writing to CAN RAM:

    The parity bits could be read in Debug/Suspend mode. The first word of the mailbox is the parity value:

  • Hello Wang,

    I really appreciate your help and response, but until now I don't see my issue yet since I'm doing almost the same thing like your code: I activate the parity in the control register and I start writing to IF1 and IF2, after writing to Cmd register for IF1 a parity issue occurs, but if I make manually a fill out of the register 0xFF1E0000 with the debugger zeros, in parity word I see 0x1F in all registers like with the yellow color of your last comment and I don't get a parity issue, so I tried to initialize the Ram message with RDA in test mode, but I get parity issue when I start the init for the message ram 00xFF1E0000 when parity is active,  I would like to ask you how to test the parity mechanism? is there any extra thing to initialize before writing to IF1 and IF2?

    I appreciate your help and thanks a lot.

    Best Regards.

    Rostom

  • Hi Rostom,

    Can you share your CCS project used for CAN RAM parity testing? 

    The data in IFx registers is transfferred to DCAN RAM only when you program the message number to CMD register. You said that the parity error occurs after writing to Cmd register (canREG1->IF1NO   = xxU;). Do you mean write message number to cmd register (canREG1->IF1NO   = xxU;)? or writing other control bits to cmd register (canREG1->IF1CMD  = (uint8) 0xF8U)?

    Did you perform the parity test using the can1ParityCheck() generated by HALCoGen?

  • Hello Wang,

    I'm using WinIdea 2012 and not code composer, so I don't have can1ParityCheck() generated by HALCoGen to test with.

     I'm doing exactly like this:

    Reg1->Ctrl &= ~(0x00001400U)

    Reg1->test = 0x00000000U

    Reg1->IF1.arb = 0x00000000U

    Reg1->IF1.msk = 0xFFFFFFFFU

    Reg1->IF1.mctl = 0x00000480U

    Reg1->IF1.data_a = 0x00000000U

    Reg1->IF1.data_b = 0x00000000U

    Reg1->IF1.cmd = 0x00F30001U

    After the last line, I get a parity error, I tried that with different ways, for the cmd with only message number or only the only mask, arb, cntrl data a and data b, but in both ways I get a parity error directly after the first write to the cmd.

    Memory before parity error (I used DCAN2 now, but I tried also DCAN1):

    message Ram:

    Memory after parity error:

    Message Ram:

    Thank you again for your help and waiting for your response.

    Best Regards.

    Rostom

  • Hello,

    There is no problem in my test. I uses your settings. Can you clear the ES before transferring data to message RAM?

  • Hello Wang,

    Thank you again, I clear ES before transferring to message Ram, I think it's something related to CCS and WinIdea, nothing else, could please show me how do you initialize the Message Ram before starting the IF and PMD init?

    Thank you very much in advance.

    BR

    Rostom

  • Hello,

    After power cycling, I perform a HW initialization on most memories (SRAM and Peripheral RAM), then I do parity check for message RAM of all CAN modules.

    1. Initialize the memory:

    /* Enable Memory Hardware Initialization */

    systemREG1->MINITGCR = 0xAU;

    /* Enable Memory Hardware Initialization for selected RAM's */

    systemREG1->MSINENA = (0x3 << 5); //bit 5 for CAN1, bit 6 for CAN2

    /* Wait until Memory Hardware Initialization complete */

    while((systemREG1->MSTCGSTAT & 0x00000100U) != 0x00000100U){

    }

    /* Disable Memory Hardware Initialization */

    systemREG1->MINITGCR = 0x5U;

    2. Run the parity check to CAN RAM: This is to check CAN RAM parity error detection and signaling mechanism by manually flip one parity bit in Direct Memory Access mode.

           void can1ParityCheck(void)

    {
    volatile uint32 canread = 0U;
    /*SAFETYMCUSW 134 S MR:12.2 <APPROVED> "LDRA Tool issue" */
    uint32 canctl_bk = canREG1->CTL;

    /* USER CODE BEGIN (65) */
    /* USER CODE END */

    /* Disable parity, init mode, TEST mode */
    canREG1->CTL = 0x00001481U;

    /* Enable RAM Direct Access mode */
    canREG1->TEST = 0x00000200U;

    /* flip the parity bit */
    canPARRAM1 ^= 0x00001000U;

    /* Enable parity, disable init, still TEST mode */
    canREG1->CTL = 0x00002880U;

    /* Read location with parity error */
    canread = canRAM1;

    /* check if ESM group1 channel 21 is flagged */
    if ((esmREG->SR1[0U] & 0x00200000U) == 0U)
    {
    /* No DCAN1 RAM parity error was flagged to ESM */
    selftestFailNotification(CAN1PARITYCHECK_FAIL1);
    }
    else
    {
    /* clear ESM group1 channel 21 flag */
    esmREG->SR1[0U] = 0x00200000U;

    /* Disable parity, init mode, TEST mode */
    canREG1->CTL = 0x00001481U;

    /* Revert back to correct data, flip bit 0 of the parity location */
    canPARRAM1 ^= 0x00001000U;
    }

    /* Disable RAM Direct Access mode */
    canREG1->TEST = 0x00000000U;

    /* Restore CTL register */
    canREG1->CTL = canctl_bk;

    /* Read Error and Status register to clear Parity Error bit */
    canread = canREG1->ES;

    /* USER CODE BEGIN (66) */
    /* USER CODE END */
    }

    3. CAN module normal operation with or without parity enabled.

  • Hello Wang,

    Unfortunately, that also didn't work, the error occurs anyway and the interrupt is triggered, I don't know if there is an other way to solve my issue or could it be a hardware problem? or the debugger and CCS has more features in initializing the ram so no parity occurs?

    Best Regards.

    Rostom

  • We are working on this issue offline. I will close this thread.