Part Number: RM44L920
Other Parts Discussed in Thread: DRV8880
Greetings.
I would like to use a GIO pin on the RM44 to drive a tri-level pin on the DRV8880,
GIO pins can be configured as open drain outputs. What is:
- The off state leakage current of the open drain output
- Assuming the state of the output can be read via register, is the state of the open drain output directly read from the open drain pin?