Part Number: TM4C1294NCPDT
In one of our projects we are using TI’s TM4C1294NCPDTI MCU.
With this board we have sometimes a problems that we are investigating now.
I have following questions:
- Do we have to power up VDDA before VDD? In the comment taken from the datasheet of this MCU (page 1820) it is not clear enough? Anyway in our board as in the schematics of TI's evaluation board (SPMU365C) VDDA and VDD are connected to the same source.
- We have discovered that by mistake supply voltage to this MCU was ~3.085V (instead of nominal 3.3V). In the datasheet minimum voltage is 2.97V (as described on Table 27-6). What do you think it can cause us a problems in some circumstances?
- In some cases in order to get the boards working we had to reprogram (???) the boards, as we think that the boards were initially programmed. Is it possible that somehow the flash memory inside the MCU was damaged or erased? Or maybe there was some kind of locking state of this MCU?