Part Number: TMS570LS3137
Hello,
I have IAR WB IDE and TMS570 Launchpad. I try to turn on launchpad NHET Leds. However i am not able to run them. What could be the problem.
Thank you very much.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS3137
Hello,
I have IAR WB IDE and TMS570 Launchpad. I try to turn on launchpad NHET Leds. However i am not able to run them. What could be the problem.
Thank you very much.
Hi,
The N2HET pins can be used as GIO pins, so you can use the GIO APIs to set/clear/read those N2HET pins.
For example, if the LED is connected to N2HET[1] pin, the LED can be turn on using this way:
gioSetPort(hetPORT1, gioGetPort(hetPORT1) ^ 0x00000002);
My question is i am not able to download program into the TMS570 launchpad from IAR workbench. However i download with CCS. TMS570 has a problem with IAR WB could it be?