Part Number: TMS570LS3137
Hi,
My understanding of the SECDED logic used for RAM and Flash ECC can detect and correct any single bit error and detect any double bit error.
Is it possible to assess the effectiveness of the algorithm in the detection of multiple (more than 2) bit errors? Is it possible to categorise groups of multiple bit errors that it will definitely detect, for example odd or even number of bits in error?
Are there assumptions in the selection of the algorithm about the probability of more than two bits being in error?
I apologise if this information is available in the TI documentation, I had a quick look and couldn't find it.
Many thanks,
Mark.