Part Number: RM41L232
Other Parts Discussed in Thread: HALCOGEN,
Hello,
I need to use GPIO Port A, B, C for my project.
in HalCoGen i can enable Port A & assign interrupts but I did not find any way for other ports, So how to do that ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
The GIO module has 8 ports: A/B/C/D/E/F/G/H. But only port A is implemented in this device. Please refer to the device data sheet.
The NHET pins are connected I/O pins. You can use all the NHET pins as GIO. But they don't support external interrupt.
Hello Wang,
Thanks for the update, meanwhile I have written my own driver to configure SPI & CAN pins to work as GPIO without an interrupt by writing to core registers, And luckily it worked for me perfectly.
And yes same way we can do N2HET also.