Part Number: TMS570LC4357-EP
Other Parts Discussed in Thread: TMS570LC4357
Hi,
We were developing schematics based on TMS570LC4357-EP. We are have two question.
Question 1:
When we see the interface between EMIF and NOR Flash, SPNU563a, Page 811; The figure shows that, we need to interface EMIF_nDQM[1:0] to BE[1:0].
However most of the NOR flash doesn't come with BE[1:0] signals. For example, in our case, we are using "MT28EW128ABA".
Is it mandatory to interface nDQM signals?
Question 2:
From the Architecture (Datasheet, Page number 5) we can see that, EMIF is not having ECC protection. Is my understanding correct? In that case, we may need to choose a SDRAM which is having built-in ECC memory protection.