Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: Error connecting to the target: (Error -151 @ 0x0)

Part Number: TMS570LS3137

Hi ,

I am trying to flash the software in TMS570LS3137 HDK board,while doing so am getting the following error message.

Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 8.3.0.00003)

I ensured that the 12v power supply is given and usb cable is connected and in working condition.

With the same power supply and usb cable am able to flash the software in different HDK board

What could the reason for this error and can this be fixed ?


Regards,
Mahendran L