Part Number: DK-TM4C129X
Tool/software: Code Composer Studio
Hello,
I'm currently trying to get the LCD display of the DK-TM4C129x to work. I'm using CCS Version: 10.1.0.00010, Windows 10 and TivaWare_C_Series-2.1.4.178. I tried out some examples like hello_widget and qs_weather, but the LCD display ist not showing anything besides the backlight that is always on due to the jumper J35 on the DK. I checked that all the jumpers of the DK are in the factory default position. I also tried to set the DK to factory default condition by running EEPROMMassErase() and than compiling one of the examples.
I don't get any errors or warnings when I compile the examples.
Does anyone have an idea why the LCD is not showing anything?
Best regards,
Lukas