Part Number: LAUNCHXL2-TMS57012
Other Parts Discussed in Thread: HALCOGEN
Hi Team,
I'm new to working with both the TMS570xx MCUs and HalCoGen. I have expansive existing code for the Launchpad, and I need to add additional features. HalCoGen creates all of the needed .c and .h files, not just the ones directly associated with the customized configurations in HalCoGen. Is there an easy way to see the short snippets of code that I need to add to my project?
The feature I need to add is an 8MHz clock output. Would you recommend using the N2HET to toggle a GIO? If not, what approach would you recommend? Is there sample code for this?
Thanks so much,