This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SynaptiCAD location crashes HET IDE?



When trying to load an HET program in HET IDE, I had an error about a SynaptiCAD thant spanned a few message boxes.  It looked like some command line flags that gave me no clues of any kind.  It also crashed HET IDE.  Rebooting did not solve.

  I have uninstalled SynaptiCAD and reinstalled it in its the default directory.  First time I had it install somewhere clean (Program Files) instead of c:\SynaptiCAD.  It has solved the problem.

IF HET IDE uses an hardcoded location for SynaptiCAD, that is VERY VERY BAD coding.  Otherwise, something else is wrong.

Frederic P.

  • Just to follow up and close, we have confirmed with the HET IDE owner that this issue has been fixed. We also understand that there was a problem with some SynaptiCAD environment variable which wasn't showing the actual install path. Thanks for your feedback.