Part Number: TMS570LC4357
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
Hello,
When reading from SDRAM, the EMIF module issues a READ command to output the starting column address and signals the SDRAM to begin the burst read operation.
When performing a double word reading, the "ldm r12, {r0, r1}" will be used to read two 32-bit words from address starting at r12, and store the value to r0 and r1
When performing a 32-bit word reading, the "ldr r2, [r12]" will be used to read one 32-bit word from address at r12, and store the data to r2
When performing a 8-bit byte reading, the "ldrb r2, [r12, #3]" will be used to read one byte from address at r12+3, and store the data to r2