Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137-EP: EMIF Interrupt Handler

Part Number: TMS570LS3137-EP
Other Parts Discussed in Thread: HALCOGEN

Hello,

I am having trouble finding the EMIF interrupt handler in the VIM table. According to the Technical Reference Manual, if a bit in the EMIF Interrupt Masked Register is set it will send an active-high pulse to the CPU interrupt controller. I have looked through both HalcoGen and the TRF and am unable to find which VIM Address is signaled.

Overall, I am attempting to work around the Errata for EMIF#3 where when an asynchronous timeout occurs and a dummy read must be done to resolve this.

Where is this active high sent or how can I handle it?

Thanks,

David Cothran