Part Number: TM4C1294NCPDT
Hi Team,
We've received an inquiry from a customer about TM4C1294. According to him, they tried to use it with an I2C slave device that clock stretches before the ACK/NAK bit is sent and it seems the MCU cannot handle that well. He thought that it isn't allowed in high-speed I2C but that it is possible in low speed (100/400kHz) based on the information from to this link, www.i2c-bus.org/.../.
He would like to confirm if the TM4C supports clock stretching between bits or only between bytes after the ACK/NAK bit.
Regards,
Danilo