Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/LAUNCHXL2-570LC43: TMS570LC43X

Part Number: LAUNCHXL2-570LC43

Tool/software: Code Composer Studio

Hello People,

When I googled more about the project for implementing peer to peer communication between LAUNCHXL2-570LC43 & Venus GX via Ethernet, I came the conclusion that for the effective implementation could be done by implementing  MODBUS TCP communication between these two devices.

[ Question]

Is it possible to establish MODBUS TCP communication between these two devices where the LAUNCHXL2-570LC43 function as MASTER & Venus GX as SLAVE?

Which program is  to be referred?

Any help is welcome!

Magizhchi,

Padayappa

  • Hello,

    TMS570LC43x has build-in EMAC, and the Launchpad (LAUNCHXL2-570LC43) has one ethernet transceiver and one RJ45 connector. We don't have example for using Modbus over TCP/IP.

    We have a active webserver demo using LWIP: