Part Number: TM4C123GH6PM
Other Parts Discussed in Thread: EK-TM4C123GXL
Hi,
Context of the issue:
I am working with EK-TM4C123GXL board. I am using the gcc arm toolchain.
I wanted to get debug prints over the OpenOCD server using Semihosting.
I compiled the project with --specs=rdimon.specs flag in the linker and included stdio.h.
Everything from compiling to flashing the image onto the target goes well.
I have also made a call to initialise_monitor_handles(); function and checked if the __libc_init_array() is being called on startup.
I also enable arm semihosting on my OpenOCD server.
Issue:
I run into a Hardfault (Imprecise bus fault to be specific) whenever I try to execute a printf or puts function. If I remove these calls the project works fine, but with these calls I *always* get hit by the same fault.
Any comments/suggestions how I can use Arm Semihosting for this device over OpenOCD ? Any help is much appreciated.
P.S. I wish I could use the CCS for this task, but the client has given specific instructions to not do so. Please help if there's any example/suggestion with OpenOCD over GDB/Telnet only.
Thanks & Regards
Pranjal