This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] Where are the TI-RTOS Extended Release Notes for TivaC?



The TI-RTOS for TivaC release notes mentioned an "Extended Release Notes" page. Where is that?

  • The old processors.wiki.ti.com page content has been moved here

    Networking

    CCS 6.1.3 on Linux

    • TI-RTOS 2.15 and 2.16 installers also install XDCtools 3.32, which can't be used to build projects in CCS 6.1.3. The following error is displayed: "XDCTOOLS_JAVA_HOME is set, but does not appear to be a directory containing a 64-bit Java Runtime Environment (1.7 or greater): e.g., '/usr/lib/jvm/java-7-openjdk-amd64'". The workaround is to switch to XDCtools 3.31.3.43, in Project Properties->CCS General->RTSC->XDCtools version. That step has to be performed for each new CCS project.

    GCC and IAR Users

    • TI-RTOS Examples SemiHosting: Examples do not work booting from flash.
    • The TI-RTOS kernel and instrumentation examples are not getting a linker file. Simply copy one from one of the TI-RTOS driver examples.