Part Number: TMS570LC4357
Hi Experts,
can you clarify if there is no IPv6 support (UDP andTCP) for the TMS570? A customer asks since they see this as a crucial feature for certain applications.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LC4357
Hi Experts,
can you clarify if there is no IPv6 support (UDP andTCP) for the TMS570? A customer asks since they see this as a crucial feature for certain applications.
Hello Simon,
The main difference of IPv6 over IPv4 is the extended address space, that is roughly 8*10^28 times larger. An IPv4 address is composed of 4 decimal byte values in the so called dot-decimal notation, and an IPv6 address consists of 16 bytes in hexadecimal notation.
So my understanding is that the EMAC on TMS570 is able to support both IPv4 and IPv6.
Hi QJ,
Thanks for the answer. Do we provide software/driver lib support for IPv6?
Hello Simon,
Micrium TCP/IP stack supports TMS570LC43x, please check if IP6 is supported by this stack.