Part Number: TMS570LC4357-EP
Hello Team,
We are using TMS controller(TMS570LC4357-EP). We have some doubts.
1.)We are interfacing the TMS controller with Epson Display controller (S1D13513F01A100) through EMIF interface. In epson display controller datasheet it is given as ADDR[21] can be used to connect to M/R` pin. This M/R` is used to select between Display buffer and Register address space. Kindly confirm the use of EMIF_ADDR[21] for M/R` pin of display controller.
2.) There are 2 Read enables for display controller but TMS controller have only one (EMIF_RNW-J1 pin), Can we use GIO's for the purpose.
Now the design is in proto stage. Shortly will complete the schematics.
Waiting for your response.
Thank You,
Regards,
Vikas H