Part Number: TMS570LC4357
Hi,
My customer reported an unexpected error caused by “CPU Interconnect Subsystem – Global error” (ESM Group1, channel 52).
- In customer’s system, “CPU Interconnect Subsystem – Global Error” is configured to drive nError pin low.
- PMIC TPS65381 detects the nError=L, then reset TMS570LC4357 by nPORRST.
- The error happens only at device power-up just after device initialization sequence. After the device is reset(nPORRST) by TPS65381, the same initialization sequence is done again, but no error happens again.
- The error does not happens at all times. The error probability is roughly 4 times in 5 trials.
- Customer checked below registers just after “CPU Interconnect Subsystem – Global Error” and before nPORRST (caused by TPS65381).
SDC_STATUS = 0x10000000 => Reserved bit is set
ERR_USER_PARTIY =0x10000000 => Reserved bit is set
SysESR=0x8008 => PORST and EXTRST are set. CPU reset is not set. As CPU reset is not generated, the error is not related to Errata Device#48.
What is potential cause of the error?
What should be checked in customer’s system?
Thanks and regards,
Koichiro Tashiro