Part Number: BOOSTXL-EDUMKII
Other Parts Discussed in Thread: MSP-EXP430FR6989, MSP-FET, MSP-EXP430FR5994, MSP430FR6989
Hello,
I am using the MSP-EXP430FR6989 in conjunction with the BOOSTXL-EDUMKII for My Microcontrollers class.
I believe that the issue is the BOOSTXL-EDUMKII, this is due to behavior of the BOOSTXL-EDUMKII regardless of a compiled code or a code communicating to it.
When attached to the MSP-EXP430FR6989 regardless of an active running code, the BOOSTXL-EDUMKII pulses the LCD Screen, buzzer, RGB LED, and green 3V3 PWG led. (image 2 & 3)
It also caused the MSP-EXP430FR698's LED102 (green top light) to turn off on eZ-FET. (image 2&3 when attached regardless of compiled code)(image 1 when not attached and code is compiled)
When attempting to compile any code with the BOOSTXL-EDUMKII attached an error message is displayed
Error initializing emulator:
A firmware update is required for the MSP430 Debug Interface (MSP-FET430UIF / MSP-FET / eZ-FET). Click the "Update" button to update the firmware and launch your debug session (this may require several update steps).
When updated or resent the compiler resends the same error
When ignored a new error is displayed
Error initializing emulator:
Could not set device Vcc.
I also tried using the project Clean command: with the BOOSTXL-EDUMKII and MSP-EXP430FR6989, with the MSP-EXP430FR6989, and just the CCS by itself with no result.
I would like to note that this issue was present when I first attached the MSP-EXP430FR6989 and the code was not compiled.
I plugged in the cable to my computer attached the BOOSTXL-EDUMKII to the MSP-EXP430FR6989 than plugged the cable into the MSP-EXP430FR6989.
Another thing as this is a class, no other student has reported this issue happening to them.
This further leads me to believe that this may be a hardware issue on my BOOSTXL-EDUMKII, not a compatibility issue or a code issue.
I would appreciate any insight or advice to remedy this problem.