Part Number: RM44L920
Other Parts Discussed in Thread: RM48L952,
Hi ,
Can we use the FLASH API F021 v02.01.01 for RM48L952 to work as Boot Loader for RM44L920 .
What migration steps should be taken care .
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
FLASH API F021 v02.01.01 can be used for all the Hercules devices. Be aware of the differences between 2 devices:
1. different system clock speed --- PLL is configured in system.c
2. different flash wait states --- Flash is configured in system.c
3. RM48 has two flash banks, but RM44 has only one flash bank. The number of flash sectors is also different. --- separate header file flash_defines.h
You can use the functions defined in bl_flash.c for both devices.