Part Number: TM4C129ENCPDT
Other Parts Discussed in Thread: CC3100, CC3135, CC3130, CC3120
Hi,
I have developed my system using TM4C129E, TI-RTOS TIVA and CC3100 using the Wi-Fi framework.
I noticed that there are new CC31xx parts in the market (CC3120, CC3130, CC3135).
My questions are:
1) Is the CC3100 going to be obsolete soon or will it be around for the next 10 to 15 years?
2) I've already developed the firmware using this chip. If I switched to the other latest CC31xx parts, are they drop in replacements and will the TIVA TI RTOS WiFi framework still work? In other words, Do I still need to change my firmware? If the new CC31xx parts are not pin to pin drop in replacements, are they at least firmware compatible?
3) Will the TM4C product line be obsolete soon or will it be around for the next 10 to 15 years?? It seems like TI has been putting more effort on the Simplelink and MSP432 products. And I don't see much activity going on related to the TM4C. For one, TM4C used to have it's own section in the forum. Now it's under other microcontrollers. Second, there used to b a TI-RTOS tutorial with TIVA-C but now I could no longer find it anywhere. It's been replaced by TI-RTIOS intro tutorial by Mindshare. When I checked out their website, it looks like the training they offer are for MSP32 and Simplelink devices and I don't see anything pertaining to TIVA. I am just now a bit worried designing new products using this MCU.
4) Just how popular TM4C is in industry? In last 3 years, I've gone to quite a number of job interviews and not one of them uses TIVA. None of the companies I worked for in the past uses TIVA. Most of them use PIC or STM32s and one NXP. Even my current company uses STM32s. But I'm a huge fan of TI and TIVA MCU's. I'm the only one in my dept. promoting this product line. When I did a demo using TM4C129E, NDK and CC3100 with TI-RTOS during our evaluation phase, my boss and I were pleased with its performance compared to STM32 with LWIP or PIC32 and Harmony, Renesas Synergy with Netx Duo. These products are all okay and they do the job well, but in my experience, TM4C NDK and the TIVA-TI-RTOS tops it all. But I'd like to feel somewhat secured that the TIVA C and TIVA TI-RTOS are still here to stay for a long time. Any thoughts on its longevity?
Any response is very much appreciated.
Thanks.
AJ