Part Number: TMS570LC4357
Does TI provide any example for DCAN FIFO?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Suthan,
To use FIFO feature, the EOB bit of all the message objects of a FIFO buffer except the last one have to programmed to zero. The EoB bits of the last message object of a FIFO Buffer is set to 1, configuring it as the end of the block.
Please use the diagram in Figure 27-12 as an example of handling the FIFO buffer. I don't example project of using CAN FIFO buffer.