Part Number: SW-DK-TM4C123G
Other Parts Discussed in Thread: EK-TM4C1294XL
Hi All,
I am having a hard time getting a simple PWM period measure program to work and need some help.
I am supplying a 320Hz PWM to port PL0 and I want to use a capture event to measure time between two rising edges.
I am running the system at 16Mhz clock and therefore I am assuming that the timer runs off the system clock. Therefore I am hoping to measure 50000 counts/ticks between 2 rising edges.
1 tick @ 16Mhz = 0.0000000625 sec and therefore, 50000 counts is 0.003125s = 320Hz. My input is very stable. I have checked it on a scope.
I am putting my code below (Timer initialization code and the Interrupt Service Routine to capture period), which when run provides me alternate outputs of 34464 and 50000 instead of a consistent 50000. What am I doing wrong?
Eventually I am planning to measure a period for waves between 2Hz and 20Hz. How can I slow down the timer clock? I tried using the TimerPrescale function from TivaWare library but that did not work.
void InitTimer(void)
{
UARTprintf("Initializing Timer0 A\n");
// Enable and configure Timer0 peripheral.
SysCtlPeripheralEnable(SYSCTL_PERIPH_TIMER0);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_TIMER0))
{
}
//Configure the pin that the timer reads from (PL0)
SysCtlPeripheralEnable(SYSCTL_PERIPH_GPIOL);
while(!SysCtlPeripheralReady(SYSCTL_PERIPH_GPIOL))
{
}
//Configure the pin that the timer reads from (PL0)
GPIOPinConfigure(GPIO_PL0_T0CCP0);
GPIOPinTypeTimer(GPIO_PORTL_BASE, GPIO_PIN_0);
TimerDisable(TIMER0_BASE, TIMER_A); // Disable timer before configuring it
TimerConfigure(TIMER0_BASE, (TIMER_CFG_SPLIT_PAIR | TIMER_CFG_A_CAP_TIME_UP) ); // Initialize timer A to count up in edge time mode
TimerClockSourceSet(TIMER0_BASE, TIMER_CLOCK_SYSTEM); // System is set at 16MHz
// TimerPrescaleSet(TIMER0_BASE, TIMER_A, 0x20); // Unsure how this works at the moment
TimerControlEvent(TIMER0_BASE, TIMER_A, TIMER_EVENT_POS_EDGE); // Timer A records pos edge time
TimerLoadSet(TIMER0_BASE, TIMER_A, 0xFFFF); // LoadSet specifies the value upto which Timer counts
// Set the pin to use the internal pull-up. Copied from a sample project
MAP_GPIOPadConfigSet(GPIO_PORTL_BASE, GPIO_PIN_0,
GPIO_STRENGTH_2MA, GPIO_PIN_TYPE_STD_WPU);
// Registers a interrupt function to be called when timer A hits a rising edge event
TimerIntRegister(TIMER0_BASE, TIMER_A, Timer0CCP0IntHandler);
TimerIntClear(TIMER0_BASE, TIMER_CAPA_EVENT); // Make sure the interrupt is cleared
IntEnable(INT_TIMER0A); // The specified interrupt is enabled in the interrupt controller.
TimerIntEnable(TIMER0_BASE, TIMER_CAPA_EVENT); // Enable the indicated timer interrupt source.
}
//When Positive edge is hit, record the values and find the difference, output to putty
void Timer0CCP0IntHandler(void)
{
TimerIntClear(TIMER0_BASE, TIMER_CAPA_EVENT);
if (gFLAG == 0)
{
gEnd = TimerValueGet(TIMER0_BASE, TIMER_A);
gLength = gEnd - gStart;
UARTprintf("\ngEnd = %d\n", gEnd);
UARTprintf("\nLENGTH = %d\n", gLength);
gFLAG = 1;
}
else {
gStart = gEnd;
gEnd = TimerValueGet(TIMER0_BASE, TIMER_A);
gLength = gEnd - gStart;
UARTprintf("\ngEnd = %d ", gEnd);
UARTprintf("LENGTH = %d\n", gLength);
}
}