Part Number: TM4C1294KCPDT
I have been updating the Tiva flash using LM flash over Ethernet. I found a strange issue that if I change the static IP address that I have used in my program, then after an update the board doesnt function any more. Its as though the program stops running. The only change seems to be if the new IP address in the new flash file is different to the one I am using to connect and update the board.