This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS: The serial port usage problem of TMS570LS31X series Demo board

Other Parts Discussed in Thread: HALCOGEN

Tool/software: Code Composer Studio

hello,

 I want use the serial port of the demo board,I have done the following work:

1. Use HALCoGen software to generate the underlying hardware driver code, enable SCI2 driver, enable SCI/LIN Port input and output signals

2. Check the schematic diagram, connect LINRX and LINTX and ground signal,Do I need to use USB to 232 interface or USB to 485 interface connection?