This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS1224: Unable to program the Hercules MCU

Part Number: TMS570LS1224
Other Parts Discussed in Thread: HALCOGEN

Hello everyone,

I have a custom board with TMS570LS1224, and am unable to download any firmware to it.

When trying to debug with XDS110, I get the error:  Error connecting to the target: (Error -2131 @0x0) Unable to access device register.

When probed with the scope, I can see the clock being generated and some date being sent through TMS line, however, nothing is generated back on TDO line.

I have also tried to use cJTAG in 2-wire mode, however I get the same error.

I have tried to download basic firmware (LED-blink generated by HALCoGen) to the other instance of the same custom board, however, I get the same error.

I have also tried using Segger J-Link debugger also to no avail (JTAG times out)

Attached is a segment of the schematic of the custom board that was designed. TMS, TDO, TDI, and TCK with nTRST go directly to the JTAG connector.

Best regards,

Tom