Part Number: TMS570LC4357
I have two questions regarding MibSPI Timing in Slave Mode with CLOCK PHASE = 0:
- The datasheet on page 203f (Table7-39 and Figure 7-23) defines the SPICLK cycle time to be 40ns. Does this mean that SPICLK cannot operate at a nominal frequency of 25MHz due to clock uncertainties? If it can operate at 25MHz, what are the limits for clock inaccuracies?
- The same section of the datasheet does not show any timing requirements between SPICLK and SPICSn. Do none exist or are they just missing? If they are missing what are they?