Hi,
My custoomer asked about the Vcc input(disabling VREG) spec and Power-on/off sequence as below;
(1) If the internal VREG is disabled, what is the specification of "Recommended Operating Condition"; Min, Nom, Max value ?
Since there is no description about the spec for the Vcc (disabling VREG, supplied from an external source) in the TMS470MF066 Data sheet(SPNS157A).
(2) If the internal LDO is disable, how much value of the bypass capacitor is recommended to be connect to the Vcc pin?
(3) If the internal LDO is disabled(Vcc is supplied from the external source), is there any specificification for Power-on sequence with all relating pins; Vcc, Vccp, VccIOR, VccAD, RST, nPORRST ?
(4) If the internal LDO is disabled(Vcc is supplied from the external source), is there any specificification for Power-off sequence with all relating pins; Vcc, Vccp, VccIOR, VccAD, RST, nPORRST ?
(5) When Vcc is supplied from external power source, is there timing specification between Vcc and nPORRST which is equivalent to the sec 5.1 in the data sheet ?
(6) The data sheet says that "It is not recommended to use the device in an application with the Vreg disabled....."
If customer uses Vcc input(disabling VREG and supplied from external source) mode, what is exactly required to take care of glitch and any other potential issues ?
(7) Just a question about the data sheet, the MAX value of the VCCPORH is specified as 1.80[V] at the Table 5-1 in page 35. But the Vcc MAX is specified as 1.70[V] at the sec 4.2 Device Recommended Operating Conditions in the data sheet page 32. How will this case be happened ?
Please advise me about the above inquiries.
Thanks in advance and Best Regards,
KIMIZUKA