Part Number: TMS570LC4357
I am trying to transfer ~1KB form MibSpi2 and 3 to two locations the RAM, when ever these to transfers happen at the same time one fails to write data in the RAM.
Both transfers a consisting of several frames and I hoped to be able have both transfers running at the same time.
If both transfers are not overlapping in time everything works fine, however if they are overlapping the one with the higher destination address fails to write.
The RAM regions are not overlapping.
Is it possible to have both transfers running at the same time, in an interleaved manner, or do I have to make sure that they are executed non overlapping?