Part Number: TMS570LS1224
Hello everbody,
I am trying to adapt the following code written for Arm Cortex M3 for TMS570LS1224;
__attribute__((noinline)) static void prv_enable_vfp( void )
{
volatile uint32_t *cpacr = (volatile uint32_t *)0x20000000;
*cpacr |= 0xf << 20;
}
static void start_app(uint32_t pc, uint32_t sp)
{
__asm volatile ("MSR msp, %0" : : "r" (sp) : );
void (*application_reset_handler)(void) = (void *)pc;
application_reset_handler();
}
int main(void)
{
prv_enable_vfp();
}
So, how to write CMSIS Cortex-R4F Core Function/Instruction ?