Part Number: TM4C123GH6PM
Tool/software: Code Composer Studio
Hello,
I'm actually trying to flash the TM4C on my PCB, but every time I get the error message "Flash programming timed out". There are no short circuits between the pins and also the suppy voltage is on the rigth pins and ground is on ground, too. When I check the voltage in the VDDC pins (Pin 25 and 56) it says 1.5 to 1.7 V, in the Datasheet it says 1.2 V. So my question are: is this the reason why I can't flash the TM4C and does this too high voltage mean my TM4C is broken or is it better than no Voltage. And when that's my problem... does exist a way to fix this?