Part Number: TMS570LS3137
Hello
About ECC function .
If the cpu RAM area have hardware fault. can ECC function Identify this erros?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS570LS3137
Hello
About ECC function .
If the cpu RAM area have hardware fault. can ECC function Identify this erros?
Hello Whong,
The ECC detection logic can detect and correct one bit ECC error, and detect 2 bits ECC error. The root cause of an error is the fault, which can be a particle impact, or defects in some part of the memory circuit. Both are hardware fault which can be detected by ECC logic.
Most of the errors are transient errors which do not persist and are correctable by software overwrites or hardware scrubbing. They are usually caused by temporary environmental factors such as particle strikes from radioactive decay and cosmic ray-induced neutrons.