Part Number: TMS570LC4357
Hello Hercules Support-Team,
According to the documentation there are tests, that trigger the ESM and consequently the nERROR Pin. As fas as I understand it is possible to clear the detected Error by SW, by clearing the bit in the ESM Status Register 1,2 and 3 corresponding to the fault generated. After the bit is cleared the nERROR can be reset by writing 5h to the ESM Error Key Register (ESMEKR).
(Q1) Is my understanding correct?
Thank you and best regards,
Max