This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS570LS3137: HALCoGen config ADC1GROUP1 and ADC2GROUP1

Part Number: TMS570LS3137
Other Parts Discussed in Thread: HALCOGEN

Dear team,

The customer set ADC1GROUP1 and ADC2GROUP1 two interrupts in HALCoGen, but ADC2GROUP1 is always executed only once. adcGetData cannot read the value.

ADC1GROUP1 can run normally, but ADC2GROUP1 only runs once.

The ADC trigger sources are HET8 and HET10, and the time setting is greater than 1us. It can be entered smoothly with a single interrupt, but two interrupts cannot be used. The pins used cannot be read regardless of whether they use a common channel or an independent channel.

Please help.