This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432E401Y: EMAC0_IRQHandler() in Ethernet_with_lwip example

Part Number: MSP432E401Y

Hi,

I am trying to add a TCP Ethernet feature to a code in c++. I am having an issue using the tcp_output() function. It puts me to the default handler, Im assuming because it cannot find the Ethernet IRQ Handler because I had to use extern C for my UARTIRQHandlers. I found the EMAC0_IRQHandler() in the lwiplib.c file however am getting an error when using extern C.

What is the best way to incorporate the lwip library in an application that is in c++(due to classes). I tried using the treat C files as C++ option but am getting lots of errors in the lwip libraries. My biggest issue right now is the ethernet IRQ embedded in the LWIP library.