Part Number: UNIFLASH
Other Parts Discussed in Thread: PGA900
Hallo TI,
I use the XDS200 with the CCS to debug a PGA900. Here it works immovable. Now I have to program the OTP memory of the PGA900 which I want to manage with the Uniflash software. Unfortunately I cannot get a connection.
I work according to the QUICK START GUIDE and do not get the desired effect.
These are my settings.
When i start and select a hex-File i get:
It is not possible to get a connection with the XDS200 and the PGA900.
When i start the Settings i get:
Where can i get the Flash Setting or what is the mistake i make?
I Use Windows10 with 64Bit.
With friendly Regards
H.Härle