Part Number: TMS570LC4357
Hi Team,
In our application we are using MibSPI interface for communication between TMS570LC4357 and FPGA, where the FPGA is configured as master mode and the TMS570LC4357 as SLAVE.
The communication established is in 4-pin mode (i.e. SOMI, MISO, CS, CLK). where the master clock (FPGA) is 10MHZ . We have configured TMS570LC4357 system clock to 180 MHZ and peripheral clock to 30MHZ as shown below:
and used below code to configure mibSPI ( used MibSPI2) as slave ( Halcogne generated code):
void mibspiInit(void)
{
uint32 i ;
/* USER CODE BEGIN (2) */
/* USER CODE END */
/** @b initialize @b MIBSPI2 */
/** bring MIBSPI out of reset */
mibspiREG2->GCR0 = 0U;
mibspiREG2->GCR0 = 1U;
/** enable MIBSPI2 multibuffered mode and enable buffer RAM */
mibspiREG2->MIBSPIE = (mibspiREG2->MIBSPIE & 0xFFFFFFFEU) | 1U;
/** MIBSPI2 master mode and clock configuration */
mibspiREG2->GCR1 = (mibspiREG2->GCR1 & 0xFFFFFFFCU) | ((uint32)((uint32)0U << 1U) /* CLOKMOD */
| 0U); /* MASTER */
/** MIBSPI2 enable pin configuration */
mibspiREG2->INT0 = (mibspiREG2->INT0 & 0xFEFFFFFFU) | (uint32)((uint32)0U << 24U); /* ENABLE HIGHZ */
/** - Delays */
mibspiREG2->DELAY = (uint32)((uint32)0U << 24U) /* C2TDELAY */
| (uint32)((uint32)0U << 16U) /* T2CDELAY */
| (uint32)((uint32)0U << 8U) /* T2EDELAY */
| (uint32)((uint32)0U << 0U); /* C2EDELAY */
/** - Data Format 0 */
mibspiREG2->FMT0 = (uint32)((uint32)0U << 24U) /* wdelay */
| (uint32)((uint32)0U << 23U) /* parity Polarity */
| (uint32)((uint32)0U << 22U) /* parity enable */
| (uint32)((uint32)0U << 21U) /* wait on enable */
| (uint32)((uint32)0U << 20U) /* shift direction */
| (uint32)((uint32)0U << 17U) /* clock polarity */
| (uint32)((uint32)0U << 16U) /* clock phase */
| (uint32)((uint32)2U << 8U) /* baudrate prescale */
| (uint32)((uint32)16U << 0U); /* data word length */
/** - Data Format 1 */
mibspiREG2->FMT1 = (uint32)((uint32)0U << 24U) /* wdelay */
| (uint32)((uint32)0U << 23U) /* parity Polarity */
| (uint32)((uint32)0U << 22U) /* parity enable */
| (uint32)((uint32)0U << 21U) /* wait on enable */
| (uint32)((uint32)0U << 20U) /* shift direction */
| (uint32)((uint32)0U << 17U) /* clock polarity */
| (uint32)((uint32)0U << 16U) /* clock phase */
| (uint32)((uint32)29U << 8U) /* baudrate prescale */
| (uint32)((uint32)16U << 0U); /* data word length */
/** - Data Format 2 */
mibspiREG2->FMT2 = (uint32)((uint32)0U << 24U) /* wdelay */
| (uint32)((uint32)0U << 23U) /* parity Polarity */
| (uint32)((uint32)0U << 22U) /* parity enable */
| (uint32)((uint32)0U << 21U) /* wait on enable */
| (uint32)((uint32)0U << 20U) /* shift direction */
| (uint32)((uint32)0U << 17U) /* clock polarity */
| (uint32)((uint32)0U << 16U) /* clock phase */
| (uint32)((uint32)29U << 8U) /* baudrate prescale */
| (uint32)((uint32)16U << 0U); /* data word length */
/** - Data Format 3 */
mibspiREG2->FMT3 = (uint32)((uint32)0U << 24U) /* wdelay */
| (uint32)((uint32)0U << 23U) /* parity Polarity */
| (uint32)((uint32)0U << 22U) /* parity enable */
| (uint32)((uint32)0U << 21U) /* wait on enable */
| (uint32)((uint32)0U << 20U) /* shift direction */
| (uint32)((uint32)0U << 17U) /* clock polarity */
| (uint32)((uint32)0U << 16U) /* clock phase */
| (uint32)((uint32)29U << 8U) /* baudrate prescale */
| (uint32)((uint32)16U << 0U); /* data word length */
/** - Default Chip Select */
mibspiREG2->DEF = (uint32)(0xFFU);
/** - wait for buffer initialization complete before accessing MibSPI registers */
/*SAFETYMCUSW 28 D MR:NA <APPROVED> "Hardware status bit read check" */
while ((mibspiREG2->FLG & 0x01000000U) != 0U)
{
} /* Wait */
/** enable MIBSPI RAM Parity */
mibspiREG2->PAR_ECC_CTRL = (mibspiREG2->PAR_ECC_CTRL & 0xFFFFFFF0U) | (0x00000005U);
/** - initialize transfer groups */
mibspiREG2->TGCTRL[0U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)0U << 8U); /* start buffer */
mibspiREG2->TGCTRL[1U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)8U << 8U); /* start buffer */
mibspiREG2->TGCTRL[2U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)(8U+0U) << 8U); /* start buffer */
mibspiREG2->TGCTRL[3U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)(8U+0U+0U) << 8U); /* start buffer */
mibspiREG2->TGCTRL[4U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)(8U+0U+0U+0U) << 8U); /* start buffer */
mibspiREG2->TGCTRL[5U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)(8U+0U+0U+0U+0U) << 8U); /* start buffer */
mibspiREG2->TGCTRL[6U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)(8U+0U+0U+0U+0U+0U) << 8U); /* start buffer */
mibspiREG2->TGCTRL[7U] = (uint32)((uint32)1U << 30U) /* oneshot */
| (uint32)((uint32)0U << 29U) /* pcurrent reset */
| (uint32)((uint32)TRG_ALWAYS << 20U) /* trigger event */
| (uint32)((uint32)TRG_DISABLED << 16U) /* trigger source */
| (uint32)((uint32)(8U+0U+0U+0U+0U+0U+0U) << 8U); /* start buffer */
mibspiREG2->TGCTRL[8U] = (uint32)(8U+0U+0U+0U+0U+0U+0U+0U) << 8U;
mibspiREG2->LTGPEND = (mibspiREG2->LTGPEND & 0xFFFF00FFU) | (uint32)(((uint32)(8U+0U+0U+0U+0U+0U+0U+0U)-1U) << 8U);
/* Didn't copy the code which configure RAM Group */
/** - MIBSPI2 Port output values */
mibspiREG2->PC3 = (uint32)((uint32)1U << 0U) /* SCS[0] */
| (uint32)((uint32)1U << 1U) /* SCS[1] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)0U << 9U) /* CLK */
| (uint32)((uint32)0U << 10U) /* SIMO */
| (uint32)((uint32)0U << 11U); /* SOMI */
/** - MIBSPI2 Port direction */
mibspiREG2->PC1 = (uint32)((uint32)0U << 0U) /* SCS[0] */
| (uint32)((uint32)1U << 1U) /* SCS[1] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)1U << 9U) /* CLK */
| (uint32)((uint32)1U << 10U) /* SIMO */
| (uint32)((uint32)0U << 11U); /* SOMI */
/** - MIBSPI2 Port open drain enable */
mibspiREG2->PC6 = (uint32)((uint32)0U << 0U) /* SCS[0] */
| (uint32)((uint32)0U << 1U) /* SCS[1] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)0U << 9U) /* CLK */
| (uint32)((uint32)0U << 10U) /* SIMO */
| (uint32)((uint32)0U << 11U); /* SOMI */
/** - MIBSPI2 Port pullup / pulldown selection */
mibspiREG2->PC8 = (uint32)((uint32)1U << 0U) /* SCS[0] */
| (uint32)((uint32)1U << 1U) /* SCS[1] */
| (uint32)((uint32)1U << 8U) /* ENA */
| (uint32)((uint32)1U << 9U) /* CLK */
| (uint32)((uint32)1U << 10U) /* SIMO */
| (uint32)((uint32)1U << 11U); /* SOMI */
/** - MIBSPI2 Port pullup / pulldown enable*/
mibspiREG2->PC7 = (uint32)((uint32)0U << 0U) /* SCS[0] */
| (uint32)((uint32)0U << 1U) /* SCS[1] */
| (uint32)((uint32)0U << 8U) /* ENA */
| (uint32)((uint32)0U << 9U) /* CLK */
| (uint32)((uint32)0U << 10U) /* SIMO */
| (uint32)((uint32)0U << 11U); /* SOMI */
/* MIBSPI2 set all pins to functional */
mibspiREG2->PC0 = (uint32)((uint32)1U << 0U) /* SCS[0] */
| (uint32)((uint32)0U << 1U) /* SCS[1] */
| (uint32)((uint32)1U << 8U) /* ENA */
| (uint32)((uint32)1U << 9U) /* CLK */
| (uint32)((uint32)1U << 10U) /* SIMO */
| (uint32)((uint32)1U << 11U); /* SOMI */
/** - Finally start MIBSPI2 */
mibspiREG2->GCR1 = (mibspiREG2->GCR1 & 0xFEFFFFFFU) | 0x01000000U;
}
In this Configuration, while sending the data through MIBSPI we are seeing the data in the MIBSPI-RAM is written properly but FPGA was the data with MSB bit set to one.
Example: if we are transmitting 0x01, 0x02, 0x03, FPGA was receiving 0xC001, 0xC002, 0xC003...
Not sure the actual root cause which is causing this issue.We also tried the Configuring the MIBSPI-RAM to different MPU configurations like Strongly Ordered, Device shareable and write-through , but did not work.
While debugging we observed that the SPI-INTFLAGs are getting set for the bit error and data length error after transmission ( value as INTFLAGs = 0x0251)and the RxBUF/Emu is being written as 0x81000000.
But when we increase the VCLK1 Clock from 30MHZ to 90MHz (shown in fig.i), then we are not seeing this issue and no error flag is being set in INTFLAGs(shown in fig. ii). Also, RxBUF/Emu is read as 0x8000FFFF and the data is being properly receievd on the FPGA .
fig.i: -
fig. ii :-
We did also try VCLK1 with 60MHZ, but we saw bit error being set in the INTFLAGS as shown below:
Please let us know if we are missing any configuration here.