This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P4111: MSP432P4111

Part Number: MSP432P4111
Other Parts Discussed in Thread: MSP-FET

My design has both MSP430 and MSP432 on the board, previously I am using MSP-FET and J-Link Base to program them, it works, for some reason, I plan to use MSP-FET-432ADPTR to replace J-Link Base, however, the SWO is not connected to ARM 10pin connector as it is configured to other IO pin, is it accepted?

Your prompt response is highly appreciated.

Regards/Wei Tao