Part Number: TMS570LS3137
Tool/software: Code Composer Studio
Hi,
I'm currently working on Hercules board(TMS570LS3137). In this i'm doing the ethernet protocol communication with PC. For this i'm using the socket API, and i did initiated the socket api by making LWIP_SOCKET to 1 and NET_CONN 1, but after doing this i'm getting numerous errors like (:identifier is undefined , expected an expression etc..). So then i included necessary header files to reduce the errors, unfortunately only few of it got cleared and errors are still pending.
What i did is installed the GCC tool according to some guidence from the forum to enable the GCC but it is not showing any option like that.
So is there any way to clear all the errors to do the Socket API program(tcp).
Thanks in advance.