This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MSP432P4011: DMA module does not fire interrupt

Part Number: MSP432P4011

I have a weird issue going on with the DMA module: even if the transfer occurs correctly, DMA ISR is not entered.


The same architecture was working with the DMA table allocated dynamically. As its size was predetermined at program startup I reverted to the classic approach of a global array allocated in the BSS but, since then, even if the table is filled-in correctly and the transfer completes, no ISR is triggered.

(Table alignment was set to 1024 in both cases)